Is possible to do a MQX USB general purpose communication without virtual COM?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is possible to do a MQX USB general purpose communication without virtual COM?

783 次查看
raulnorthstar
Contributor II

Hi Freescale team and community.

I need to do a general purpose USB communication between Kinetis (TWR-K60 using MQX) and PC. The PC side is solved thanks to example from Freescale ("How to make a graphical user interface (GUI) for USB communication") and the extensive host drivers examples for PC. But in the microcontroller side, I am not able to do this.

I started using the good example of USB CDC Virtual COM and worked perfectly, but now, I need to do the communication without virtual COM port.

I have tried to do a new class driver using the manual "Freescale MQX USB Device User’s Guide" specifically the chapter "Chapter 4 Developing new Class Drivers", but it has a very short explanation and there are not any examples for to do a complete new class driver. Also I have tried to move the micro side code from Freescale example (How to make a graphical user interface (GUI) for USB communication) and neither I have been able.

I need some help with this theme and if somebody has an example, I would be greatful. Thanks!

标签 (1)
标记 (1)
0 项奖励
回复
0 回复数