Is MQX supports IGMP for Multicasting?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is MQX supports IGMP for Multicasting?

ソリューションへジャンプ
3,020件の閲覧回数
AloysiusJegan
Contributor III

Is MQX version 3.1 or 3.2 supports IGMP protocol for multicasting?

If yes, can anyone tell me how to configure it?

 

Thanks.

 

-Jegan

0 件の賞賛
返信
1 解決策
1,526件の閲覧回数
AloysiusJegan
Contributor III

RTCS stack supports IGMP (It took nearly 1 week for me to identify the support)....

 

 

95% of my questions was answered by myself only. What you feel?

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,526件の閲覧回数
flashtoo
Contributor I

I had to rebuild the library to get IGMP work. Contrary to what the documentation implies it is not enabled by default. If not part of the library, you will get an error that it can't find "SOL_IGMP_CALL" when trying to use "SOL_IGMP" to set socket options (assuming you are using BSD model). Open project for your development board (rtsc_m52259evb) find user_config.h and add "#define RTCSCFG_ENABLE_IGMP      1" in the "board-specific RTCS settings" section.

 

I can then send and receive multicast messages. Having said that, I don't seem to be seeing any membership reports being sent out. More to come as I'm still evaluating this...

 

PS, this logically belongs in the RTCS section of this Forum

 

Bill

0 件の賞賛
返信
1,526件の閲覧回数
AloysiusJegan
Contributor III

I am using MQX 3.3 version. I am able to send and reecive membership report using the RTCS stack available there.

 

 

-AJ

 

http://www.aloysiusjegan.in

0 件の賞賛
返信
1,527件の閲覧回数
AloysiusJegan
Contributor III

RTCS stack supports IGMP (It took nearly 1 week for me to identify the support)....

 

 

95% of my questions was answered by myself only. What you feel?

 

 

 

0 件の賞賛
返信