I am trying to update a project using MQX 3.7 to use MQX 4.2.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I am trying to update a project using MQX 3.7 to use MQX 4.2.

2,194 Views
gopher
Contributor I

I am trying to update a project running on a Freescale MK10DN512VLQ10 using MQX 3.7 to use MQX 4.2.  I went through the cloning process using twrk60n512 as the base and am running into a lock up situation.  In bsp_cm.c, when we go into __pe_initialize_hardware, things seem to be fine until we hit the line setting MCG_C2.  Since it's the same processor, why is it setting different values for MCG_C2 and MCG_C1 vs. what it was setting in MQX 3.7?

_bsp_watchdog_disable();

/*** !!! Here you can place your own code before PE initialization using property "User code before PE initialization" on the build options tab. !!! ***/

/*** ### MK40DX256ZVMD10 "Cpu" init code ... ***/
/*** PE initialization code after reset ***/
/* System clock initialization */
/* SIM_SCGC5: PORTA=1 */
SIM_SCGC5 |= (uint32_t)0x0202UL; /* Enable clock gate for ports to enable pin routing */
if ( *((uint8_t*) 0x03FFU) != 0xFFU) {
MCG_C3 = *((uint8_t*) 0x03FFU);
MCG_C4 = (MCG_C4 & 0xE0U) | ((*((uint8_t*) 0x03FEU)) & 0x1FU);
}
/* SIM_CLKDIV1: OUTDIV1=0,OUTDIV2=1,OUTDIV3=1,OUTDIV4=3,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */
SIM_CLKDIV1 = (uint32_t)0x01130000UL; /* Update system prescalers */
/* SIM_CLKDIV2: USBDIV=1,USBFRAC=0 */
SIM_CLKDIV2 = (uint32_t)((SIM_CLKDIV2 & (uint32_t)~0x0DUL) | (uint32_t)0x02UL); /* Update USB clock prescalers */
/* SIM_SOPT2: PLLFLLSEL=1 */
SIM_SOPT2 |= (uint32_t)0x00010000UL; /* Select PLL as a clock source for various peripherals */
/* SIM_SOPT1: OSC32KSEL=1 */
SIM_SOPT1 |= (uint32_t)0x00080000UL; /* RTC oscillator drives 32 kHz clock for various peripherals */
/* PORTA_PCR18: ISF=0,MUX=0 */
PORTA_PCR18 &= (uint32_t)~0x01000700UL;
/* Switch to FBE Mode */
/*
** [ENGR288288] Only enable External reference in Low Power Mode
** There is a conflict between VLLSx and GPIO on TWR-K60N512: XTAL and SW1 are using PTA19
** If enable external reference clock (OSCERCLK) and allow it working on STOP mode,
** PTA19 can't be used as input (refer to 10.2.3 section in RM)
*/
#if MQX_ENABLE_LOW_POWER
/* OSC_CR: ERCLKEN=1,??=0,EREFSTEN=1,??=0,SC2P=0,SC4P=0,SC8P=0,SC16P=0 */
OSC_CR = (uint8_t)0xA0U;
#else
/* OSC_CR: ERCLKEN=0,??=0,EREFSTEN=0,??=0,SC2P=0,SC4P=0,SC8P=0,SC16P=0 */
OSC_CR = (uint8_t)0x00U;
#endif
/* SIM_SOPT2: MCGCLKSEL=0 */
SIM_SOPT2 &= (uint32_t)~0x01UL;
/* MCG_C2: ??=0,??=0,RANGE=2,HGO=0,EREFS=0,LP=0,IRCS=1 */
MCG_C2 = (uint8_t)0x21U;
/* MCG_C1: CLKS=2,FRDIV=5,IREFS=0,IRCLKEN=0,IREFSTEN=0 */
MCG_C1 = (uint8_t)0xA8U;
/* MCG_C4: DMX32=0,DRST_DRS=0 */
MCG_C4 &= (uint8_t)~(uint8_t)0xE0U;
/* MCG_C5: ??=0,PLLCLKEN=0,PLLSTEN=1,PRDIV=0x18 */
MCG_C5 = (uint8_t)0x38U;
/* MCG_C6: LOLIE=0,PLLS=0,CME=0,VDIV=0x18 */
MCG_C6 = (uint8_t)0x18U;
while((MCG_S & MCG_S_IREFST_MASK) != 0x00U) { /* Check that the source of the FLL reference clock is the external reference clock. */
}
while((MCG_S & 0x0CU) != 0x08U) { /* Wait until external reference clock is selected as MCG output */
}

0 Kudos
Reply
7 Replies

1,774 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Eric:

There are two bsps for K60 in MQX 4.2, one is K60N512 (Rev 1.x, old version), the other is K60D100M (Rev2.x), the MCG_C2 is different, please see below.

pastedImage_1.png

K60D100M features the MK60DN512VMD10, maybe similar to your chip. 

I would suggest you use BSP for TWR-K60D100M as the clone base and try it again.

Regards

Daniel

--------------------------------------------------------------------------------------------

If this post is helpful please click correct or helpful answer, thank you!

0 Kudos
Reply

1,774 Views
gopher
Contributor I

Hi Daniel -

Today I tried doing that, but I see the same kind of failure.  The code is a bit different now, this time the issue comes up when it hits the line setting MCG_C7 and if I put a watch on it, is says it's undefined but I can see things like MCG_C1, MCG_C2, etc. so I suspect that I actually do have a Rev. 1.0.

Going back to the original issue, when we get to the line where we first set MCG_C2 to 0x21, I stepped through the disassembly and saw that the MOVS command successfully writes the 0x21 into R0, and then the LDR.N command successfully writes 0x40064001 (the address of MCG_C2) into R1.  The problem comes with the STRB command which should write the value in R0 into R1.  When I process that step, the disassembly jumps me back to 0x0 and it locks up.   Is that likely because there's some kind of issue with writing that value to that register?

0 Kudos
Reply

1,774 Views
danielchen
NXP TechSupport
NXP TechSupport

what is the mask set of your MCU?  you can get it from the MCU. For example, the mask set of mine K60n512 is 0M33z.

0 Kudos
Reply

1,774 Views
gopher
Contributor I

There are chips of varying ages in the devices I'm working on - the ones I have for testing have 2N30D, 4N30D or 8N30D.

0 Kudos
Reply

1,774 Views
danielchen
NXP TechSupport
NXP TechSupport

Yes, the chips you are working are Rev. 1.x.

Please refer to the below two links for reference

Creating MQX 4.0 BSP for K10 

https://community.nxp.com/message/384366 

I hope it helps

Regards

Daniel

--------------------------------------------------------------------------------------------

If this post is helpful please click correct or helpful answer, thank you!

0 Kudos
Reply

1,774 Views
gopher
Contributor I

I'll keep working on it.  Are mask sets 4N22D and 5N22D both Rev 2.x?

0 Kudos
Reply

1,774 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Eric Thrall

Yes,  both are Rev 2.x

Regards

Daniel

--------------------------------------------------------------------------------------------

If this post is helpful please click correct or helpful answer, thank you!

0 Kudos
Reply