How to build BSP/PSP/library in S32DS IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to build BSP/PSP/library in S32DS IDE

1,378件の閲覧回数
jianlongzhang
NXP Employee
NXP Employee

Dear All,

I downloaded MQX 4.2 for Halo Rev 6 package and wanted to run examples in S32DS. Fortunately, there is few description about how to build BSP/PSP library in S32DS only below information.

pastedImage_1.png

Firstly, I import project '\MQX_4_2_Halo_0_6\mqx\build\s32ds\bsp_mac57d5mb\bsp_mac57d5mb_A5' to S32DS, but failed to build, error shown below.

pastedImage_6.png

Could anyone help me build BSP and PSP in S32DS, thank you very much!

Best Regards

Tony Zhang

0 件の賞賛
返信
2 返答(返信)

1,175件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Tony:

My understanding is you need to import the application workspace, then you can build the BSP liabrary and PSP library.

For example, in classic MQX 4.2, if you need to build hello world with frdmK64f board, you can import the hello world workspace.

Freescale_MQX_4_2\mqx\examples\hello\build\kds\hello_frdmk64f

I also suggest you can ask a S32 related question in S32 space

https://community.nxp.com/community/s32/s32ds 

Regards

Daniel

0 件の賞賛
返信

1,175件の閲覧回数
jianlongzhang
NXP Employee
NXP Employee

Hi Daniel,

Thank you very much!

Yes, I have imported project '\MQX_4_2_Halo_0_6\mqx\build\s32ds\bsp_mac57d5mb\bsp_mac57d5mb_A5' to workspace and failing to build.

Do you think if there is any other configuration I need to do?

Thanks.

Best Regards

Tony

0 件の賞賛
返信