How to Develop Graphics LCD (128x64 dot matrix NT7108C - Driver) MQX RTOS Project on TWR‐K60D100M board and Library files for the same

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Develop Graphics LCD (128x64 dot matrix NT7108C - Driver) MQX RTOS Project on TWR‐K60D100M board and Library files for the same

2,173件の閲覧回数
abhishekinamdar
Contributor II

Hello Everyone

     How to Develop Graphics LCD (128x64 dot matrix NT7108C - Driver) MQX RTOS Project on TWR‐K60D100M board and Library files for the same. We dont want to used the Tower LCD module instead we have "Newhaven Display_NHD‐12864MZ‐FSW‐GBW‐L". Need to develop the Menu Structure with the Keyboard Interphase, thats secondary. First we need to control and display different parameter on Graphics LCD as described above on TWR‐K60D100M board. Please provide help.

Regards

Abhishek

ラベル(1)
0 件の賞賛
2 返答(返信)

934件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

If you are planing to use eGUI, you need to write your own LCD driver for the controller.

Check : D4D\low_level_drivers\LCD\lcd_controllers_drivers

You have there a template for the new controller driver.

You could reuse the hw interface also in D4D\low_level_drivers\LCD\lcd_hw_interface

like flexbus for the K60.

Luis

0 件の賞賛

934件の閲覧回数
abhishekinamdar
Contributor II

Hello Luis,

     Thanks for the reply, We are new to work on the LCD Menu structure development. Developing the Drivers from scratch would be tough for us, we need some head start or example, before we begin. And we have the following doubts:

1. Firstly it is not mandatory to use eGUI, we just have to use TWR‐K60D100M board, Newhaven Display_NHD‐12864MZ‐FSW‐GBW‐L and MQX RTOS for the development of the controller with menu strucuture. So we can use any available library's for the above mentioned hardware. Please suggest if any file/library available.

2. We searched through the internet for the Low level Monochrome LCD Menu structure Lib available for the MQX we found D4CD (Gargy007/D4CD · GitHub ) an modify version of eGUI(D4D). We thought to use D4CD, any suggestion on the same.

3. Please provide any examples for the above two methods(D4D / D4CD), if you have any, for Monochrome GLCD 128x64 Menu structure development with above hardware, for the head start. :smileyhappy:

Thanks for your time..

Regards

Abhishek

0 件の賞賛