I have installed KDS_1.1.1 and MQX 4.1.1. I have imported the twrk60f120m workspace and built the libraries. When I try to create a new project to use the MQX libraries, there is no obvious wizard or option that allows me to do that. Is that handled differently in KDS than it is in CodeWarrior 10.6 or is it not possible yet?
已解决! 转到解答。
Hi,
Official support of KDS in MQX is planned in MQX 4.2 & MQX 5.0 coming later this year.
At that time MQX plug-ins for KDS (e.g. Task Aware Debug & New Project Wizard) will be available. Also, MQX project files for all libraries and examples will be available for KDS.
Alice
Best Regards
Hi Kelly,
Unfortunately there is not an option in KDS wizard to create MQX for KSDK project, I recommend to make a copy of an existing demo or example and edit this project. You can find them in the following paths.
C:\Freescale\MQX_KSDK_1.0.0\demos
C:\Freescale\MQX_KSDK_1.0.0\rtos\mqx\mqx\examples
Hope this helps.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Official support of KDS in MQX is planned in MQX 4.2 & MQX 5.0 coming later this year.
At that time MQX plug-ins for KDS (e.g. Task Aware Debug & New Project Wizard) will be available. Also, MQX project files for all libraries and examples will be available for KDS.
Alice
Best Regards