Hi,
working in MQX I don't understand how I can insert my ISR that use DMA timer 0.
I'm using M52259EVB with MQX_ROM_VECTOR 0, is DMA timer 0 interrupt already used by MQX RTOS? Can I use this interrupt for my application?
Solved! Go to Solution.
Hi, look at the following post, perhaps it can help you.
Thanks for the support.
With this code now the interrupt is running in MQX but I have to set the DTIM3 manually ... can I do it or should I use MQX routines?
static void (_CODE_PTR_ old_isr_dtim3)(pointer);
MCF_DTIM3_DTMR = BASE_TIMER_CLK_BUS_1 | BASE_TIMER_PRESCALER_1 | BASE_TIMER_RESET_AFTER_MATCH | BASE_TIMER_INT_ENABLED | BASE_TIMER_DISABLED;
MCF_DTIM3_DTXMR = BASE_TIMER_STEP_1 | BASE_TIMER_CONTINUE_HALTED | BASE_TIMER_DMA_REQUEST_DISABLED;
MCF_DTIM3_DTRR = BASE_TIMER_REFERENCE_VALUE;
MCF_DTIM3_DTER |= (uint_8)0x03; //Clear reference flag
old_isr_dtim3=_int_install_isr(MCF5225_INT_DTIM3, (void (_CODE_PTR_)(pointer))isrINT_DTIM3, NULL);
MCF_INTC0_ICR22 = (uint_8)((DTIM3_INTERRUPT_LEVEL << 3) | DTIM3_INTERRUPT_PRIORITY);
MCF_INTC0_IMRL &= ~IMRL3_TBASE_MASK;
if (NULL == old_isr_dtim3)
return IO_ERROR; /* could not install new interrupt routine */
MCF_DTIM3_DTMR |= (uint_16)0x0001; //Timer start
This code is all right from functionality point of view, nothing must be changed. I was not checking DTIM settings.
Hi, look at the following post, perhaps it can help you.