Hi
I think you can change the BSP header file. For example , for my board, the header file is
C:\Freescale\Freescale_MQX_4_2\mqx\source\bsp\twrk20d72m\twrk20d72m.h
/*
** TTYA and ITTYA baud rate
** MGCT: <option type="number" min="0" max="115200"/>
*/
#ifndef BSPCFG_SCI0_BAUD_RATE
#define BSPCFG_SCI0_BAUD_RATE 115200
#endif
Regards
Daniel