HTTPSRV MQX 4.02 and CW10.2 with MCF52259

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HTTPSRV MQX 4.02 and CW10.2 with MCF52259

1,392 Views
YodaC
Contributor III

Hi,

I try to change HTTPD to HTTPSRV, because HTTPD is very bad with IE.

The firsts tests crashes.

I had to change HTTPSRV_SERVER_STACK_SIZE from 850 to 1000 and HTTPSRV_SESSION_STACK_SIZE from 1300 to 1500  in httpsrv_prv.h to avoid crash.

Now, the problem is that some files are aborted  when the web browser try to open the web pages.

This is the same with Firefox an IE.

 

What can i do to have files to be downloaded correctly ?

Does anybody make run HTTPSRV on a MCF5225X ?

0 Kudos
Reply
3 Replies

1,224 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Christian,

I am able to run HTTPSRV in TWR-MCF52259 with MQX4.2.0.2.

Just me aware of the jumper settings required in TWR-SER. You can find this settings in chapter 9.21 TWR-MCF52259 of MQX_Getting_Started.pdf which is located in the following path:

C:\Freescale\Freescale_MQX_4_2\doc

Best regards,

Carlos

0 Kudos
Reply

1,224 Views
YodaC
Contributor III

Thank you Carlos,

I try to use MQX 4.02, because I can't  compile MQX 4.2 with my licensed CW10.2.

Best regards,

Christian

0 Kudos
Reply

1,224 Views
Carlos_Musich
NXP Employee
NXP Employee

Christian,

In this case I recommend to submit a Service Request at www.freescale.com/support to ask if your license can be upgraded.

Regards,

Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply