Hi guys.
I am doing an ADC code in MQX for FRDMK64. I used the LWADC example and made some changes an the code is working. But i want the ADC to run in full speed. I tried to change the clock by using
_lwadc_set_attribute(&lwadc_inputs[i],LWADC_FREQUENCY,12000000);
but after this command when i am printing this clock to see whether it changed. it shows 8Mhz clock.
I tried to change the vref using this function then there is no change but whe i changed it in the BSP it is working.
#define BSP_ADC_VREF_DEFAULT (3300)
But i dont know where to change the ADC clock in BSP.
Please help
Regards,
Olivia
解決済! 解決策の投稿を見る。
Hi Olivia:
In current LW ADC driver , LWADC_FREQUENCY value should be set in the API _lwadc_init . this value can't be changed with _lwadc_set_attribute.
Please check this API, there is a table made from the datasheet
const static uint32_t adc_max_frq_table[] = {
2500000, /* 2.5 MHz for low power, normal speed, 16b resolution */
5000000, /* 5.0 MHz for low power, normal speed, lower resolution */
5000000, /* 5.0 MHz for low power, high speed, 16b resolution */
8000000, /* 8.0 MHz for low power, high speed, lower resolution */
8000000, /* 8.0 MHz for normal power, normal speed, 16b resolution */
12000000, /* 12.0 MHz for normal power, normal speed, lower resolution */
12000000, /* 12.0 MHz for normal power, high speed, 16b resolution */
18000000, /* 18.0 MHz for normal power, high speed, lower resolution */
};
If you want to use 12M, please change line 127
if (init_ptr->POWER == LWADC_LPC_NORMAL)
adc_max_frq_index |= 0x04;
to
adc_max_frq_index |= 0x05;
I hope it helps
Have a great day,
Daniel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Olivia:
In current LW ADC driver , LWADC_FREQUENCY value should be set in the API _lwadc_init . this value can't be changed with _lwadc_set_attribute.
Please check this API, there is a table made from the datasheet
const static uint32_t adc_max_frq_table[] = {
2500000, /* 2.5 MHz for low power, normal speed, 16b resolution */
5000000, /* 5.0 MHz for low power, normal speed, lower resolution */
5000000, /* 5.0 MHz for low power, high speed, 16b resolution */
8000000, /* 8.0 MHz for low power, high speed, lower resolution */
8000000, /* 8.0 MHz for normal power, normal speed, 16b resolution */
12000000, /* 12.0 MHz for normal power, normal speed, lower resolution */
12000000, /* 12.0 MHz for normal power, high speed, 16b resolution */
18000000, /* 18.0 MHz for normal power, high speed, lower resolution */
};
If you want to use 12M, please change line 127
if (init_ptr->POWER == LWADC_LPC_NORMAL)
adc_max_frq_index |= 0x04;
to
adc_max_frq_index |= 0x05;
I hope it helps
Have a great day,
Daniel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------