GainSpan GS2100M with K66

cancel
Showing results for 
Search instead for 
Did you mean: 

GainSpan GS2100M with K66

376 Views
arielablumer
Contributor III

I'm integrating Gain Span 2100M into a K66 platform and encountering stability issues.

It happens that the debugger is reset or that the SW is looping forever in _lwmem_get_next_block_internal within a do while where block_ptr->BLOCKSIZE equals 0.

According to the stacl, this function is called from _task_destory which should not have been activated in regular flow.

My questions are:

- Are there any known issues w/ this integration?

- When was the last GS driver released? how can I download it?

Thanks,

Ariela

0 Kudos
1 Reply

154 Views
soledad
NXP Employee
NXP Employee

Hello Ariela,

The WiFi board and MQX patches are developed by our partnr GainSpan. They have not developed patch for the latest MQX release.

Please check the below threads these may help!

Porting the Gainspan application from MQX 3.7 to MQX 4.0

https://community.freescale.com/thread/304770#318565

Recompile the MQX

TWR-WIFI-G011M1 with TWR-60K and TWR-SER


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos