Freescale_MQX_4_1_1_IP6_EVAL with DHCP & SNTP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale_MQX_4_1_1_IP6_EVAL with DHCP & SNTP

757 Views
daweiyou
NXP Employee
NXP Employee

Hi:

I download RTCS IPv6 Evaluation package (Freescale_MQX_4_1_1_IP6_EVAL directory) , and could build and run basic shell command from shell.

But I still would like to check whether SNTP and DCHP are supported in this evaluation package?

And If they exist, how I write demo code to test them? thx.

Labels (1)
0 Kudos
Reply
1 Reply

650 Views
RadekS
NXP Employee
NXP Employee

Hi Dawei,

unfortunately SNTP is currently supported only for IPv4 and DHCP client for IPv6 was added from MQX version 4.2.0.

I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply