Forcing 10 Mbps Ethernet Connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Forcing 10 Mbps Ethernet Connection

跳至解决方案
1,861 次查看
rdazcal
Contributor III

Greetings,

 

Is there a parameter where I can force RTCS to establish a 10 Mbps (10Base-T) even if the network supports 100 Mbps connections (100Base-TX)?

 

Also, if I do so, are there 100Base-TX only networks? I suppose a 10Base-T should work in any network, correct?

 

I need this in order to save power in my end-device

 

Thank you

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,088 次查看
rdazcal
Contributor III

If anyone is interested, here is a link for the solution in another thread: https://community.freescale.com/thread/72070

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,089 次查看
rdazcal
Contributor III

If anyone is interested, here is a link for the solution in another thread: https://community.freescale.com/thread/72070

0 项奖励
回复