Flash Programming using Ethernet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash Programming using Ethernet

973 次查看
utsavikalpesh
Contributor V

Hi,

I am working with TWRK60D100M kit using Codewarrior v10.6 and of mqx v4.0.

Rightnow, I am using USB Multilink universal to download code.

Now my requirement is to download a code using Ethernet Cable.

Can anybody tell me what exactly I need to do???

0 项奖励
回复
1 回复

856 次查看
soledad
NXP Employee
NXP Employee

Hello,

You can use an Ethernet bootloader, please check the below application note:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4367.pdf

This document describes how to use an Ethernet bootloader provided by Freescale. It explains how to modify the .lcf and .icf link files of CW and IAR IDEs respectively, in order to add the Ethernet bootloader support for your application.

In addition please check the below link: (Green Hills Probe:)

Hardware Debuggers and Programming Interfaces|Freescale


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复