Hello all,
I´m using Coldfire MCF52258AG80 hardware with MQX 3.4 (planning to upgrade).
My question is:
¿Is it possible to find how much static RAM (SRAM) memory my program (together with MQX) is consuming?
That is, counting MQX memory, global, static and stack variables, tasks stack size, dynamically allocated variables, etc. Everything.
Because I need to know if certain functionality which I need to add fits into SRAM.
Thank you in advance,,
David.
已解决! 转到解答。
Hi David,
If you have the CW professional you have access to the TAD (Task Aware Debugging) that allows you to see the head (SRAM) useage. You simple run your application and halt/stop/break at some point to allow the debugger to upload the information and display it
Look at the following PDF in the MQX path starting on page 50 for some of the TAD features.
Freescale MQX3.7\doc\FSL_MQX_3_7_in_CW_10_1.pdf
Hope this helps.
Regards,
David