Feature Request for Kinetis: DMA for UARTs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Feature Request for Kinetis: DMA for UARTs

1,106 次查看
Fabi
Contributor III

It would be great, if DMA will be supported for UARTs. The use-case is to send and receive about 100 Bytes every 5 msec with 460 KBaud. Using ittya: is my current solution, but it decelerates the system noticeable.

PLS, could freescale add it into the feature request list for MQX 3.9 or 4.0?

0 项奖励
回复
2 回复数

778 次查看
KJFPE
Contributor III

Try the USB virtual comm port which will be able to go at the speed you require

0 项奖励
回复

778 次查看
Fabi
Contributor III

@HJFPE Thanks for the hint. The use case is, however, inter processor communication inside an embedded device. SPI is not an option (because of reduced feature set of the other processor) as well as USB, too.

0 项奖励
回复