FXLC95000 Evaluation Kit question / MQX 3.7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FXLC95000 Evaluation Kit question / MQX 3.7

292 Views
ryandeville
Contributor I

Hello All,

I'm trying to recompile the MQX 3.7 BSP for the FXLC95000 Evaluation Kit to enable the I2C master.  My problem is when I recompile the BSP with the user_config.h file with the line

#define BSPCFG_ENABLE_I2C0          1

an error is generated in the i2c_fxlc95000.c file, complaining of undefined identifiers FXLC95000_INT_Viic1 on line 84, similar for lines 87, 55, 58.  Usually these types of errors are because an include file did not get included or a path error.  But I have tried grepping for the above string on the mqx/source path, and the only file that comes back with this identifier is the i2c_fxlc95000.c file...this doesn't seem to be defined anywhere I can find.

To recreate:

Use CodeWarrior 10.5

Download ISF 1.1 from freescale site: XTRINSIC_ISF: Xtrinsic Intelligent Sensing Framework

Update the MQX 3.7 for the evaluation kit: XTRINSIC_ISF: Xtrinsic Intelligent Sensing Framework

(from the download page)

Follow the steps in AN4287 to create custom BSP based upon the FXLC95000eval

Modify line in user_config.h

Attempt to compile BSP

Explode

Thanks.

Tags (1)
0 Kudos
0 Replies