FFS Mutex problem.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FFS Mutex problem.

881 次查看
danielchai
Senior Contributor I

Hi All,

Now I installed the FFS patch on MQX4.0.2 on TWRK60F120M.

And I installed the wear leveling without installing MFS on NAND FLASH.

When I try to use read/write NAND FLASH in a interrupt, it prints: "assertion failed: 0, file simple_mutex.cpp, line 141".

After digging into it, I found it can not lock the mutex because it can lock the mutex in a interrupt.

Do anyone have any ideas how can use read/write based on FFS in a interrupt?

Thank you.

-Daniel

0 项奖励
回复
0 回复数