Error opening part MGR(0x30aa) PMGR INVALID PARTITION

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error opening part MGR(0x30aa) PMGR INVALID PARTITION

1,155 次查看
JKadin
Contributor II

I am trying to use an external SPI flash to store my web page data on a TWRMCF52259.

 

I have the SPI FLASH working using the BSP's spi0  and MQX fopen ("spi0:", NULL)

 

I can read, write, and erase the flash using this method.

 

I created an io device and can do freads and fwrites on the device.

 

I am up up to layering on the partition manager and the install works  and returns a valid partition handle.

     error_code = _io_part_mgr_install(webflsh_handle, partman_name, SPI_MEMORY_PAGE_SIZE);

The fopen returns a valid handle

                 partman_handle = fopen(partman_name, NULL);

 

 

I am failing on the  IO_IOCTL_VAL_PAR with the invalid partition error, which I think is normal since the device is erased.  I also traced through the code which does a read of address 0 and then does not find the correct data to indicate a valid partition.

     error_code = _io_ioctl(partman_handle, IO_IOCTL_VAL_PART, &param);

ERROR(0x30aa) PMGR INVALID PARTITION

 

Because I got INVALID_PARTITON I thought I need to set the partition first so I tried

         error_code = _io_ioctl(partman_handle, IO_IOCTL_SET_PARTITION, NULL);

 which returns the same error

Error creating part MGR(0x30aa) PMGR INVALID PARTITION

 

Does anyone know if this is how you are supposed to do it, I have not found any examples that call IO_IOCTL_SET_PARTITION and have not figured out how to format before the partition manager is running.

Thanks

 

 

 

 

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

881 次查看
PetrM
Senior Contributor I

Hello,

 

format command should set up sector 0 with default partition.

If it doesn't work, try it without using partition manager first.

 

PetrM

 

0 项奖励
回复