Error during debugging for Hexiwear using KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error during debugging for Hexiwear using KDS

2,581件の閲覧回数
markjvillamor
Contributor I

Good evening,

I am currently programming Hexiwear using KDS. I followed the startup instructions carefully and I did not encounter any problems building the program at gitub. I then moved on to debugging and it was going smoothly at first before I encountered this error message. The debugger was loading up until 8% before having issues as seen in the image. Has any of you encountered and solved this problem?

Thank you.

Mark

PyOCD.JPG

0 件の賞賛
返信
1 返信

2,448件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the following thread:

https://community.nxp.com/thread/506007 

I hope this helps, have a nice day!

Regards

Soledad

0 件の賞賛
返信