EDS Client Tool - Plans to include in future MQX releases?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EDS Client Tool - Plans to include in future MQX releases?

ソリューションへジャンプ
1,433件の閲覧回数
pmt
Contributor V

 

Will EDS Client make it into a future Freescale MQX distribution?  This is a critical troubleshooting tool for live systems.  This is especially true when JTAG connections are not possible and only Ethernet links are available.

 

 

 

 

0 件の賞賛
返信
1 解決策
1,254件の閲覧回数
c0170
Senior Contributor III
0 件の賞賛
返信
2 返答(返信)
1,255件の閲覧回数
c0170
Senior Contributor III

Hi pmt,

 

do you mean this tool? http://www.embedded-access.com/products/host_tools.html

 

Regards,

MartinK

0 件の賞賛
返信
1,254件の閲覧回数
pmt
Contributor V

Yes, 

 

MQXDebug EDS Client.  This is not in the current distribution of Freescale MQX per the release notes.

 

Just talked to EA.  Appartently this will be released at some point in the future as an Eclipse plugin.

 

Chris

0 件の賞賛
返信