EDS Client Tool - Plans to include in future MQX releases?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EDS Client Tool - Plans to include in future MQX releases?

Jump to solution
1,377 Views
pmt
Contributor V

 

Will EDS Client make it into a future Freescale MQX distribution?  This is a critical troubleshooting tool for live systems.  This is especially true when JTAG connections are not possible and only Ethernet links are available.

 

 

 

 

0 Kudos
Reply
1 Solution
1,198 Views
c0170
Senior Contributor III
0 Kudos
Reply
2 Replies
1,199 Views
c0170
Senior Contributor III

Hi pmt,

 

do you mean this tool? http://www.embedded-access.com/products/host_tools.html

 

Regards,

MartinK

0 Kudos
Reply
1,198 Views
pmt
Contributor V

Yes, 

 

MQXDebug EDS Client.  This is not in the current distribution of Freescale MQX per the release notes.

 

Just talked to EA.  Appartently this will be released at some point in the future as an Eclipse plugin.

 

Chris

0 Kudos
Reply