Does support USB Host isochronous transfer mode supported

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does support USB Host isochronous transfer mode supported

Jump to solution
1,405 Views
isaotakashima
Contributor IV

I want to make new project to support USB isochronous transfer using KL26 device.

Does MQX's USB host driver for KL26 support isochronous transfer mode?

Please reply as soon as possible.

Best regards,

Takashima

0 Kudos
Reply
1 Solution
1,092 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Takashima:

Yes, the KL26 device supports isochronous transfer. But due to the limited flash size, the host_audio_speaker example is not enabled for KL26. You can refer to the host_audio_speaker example of some other platforms, ie.K22, to try isochronous transfer.

Regards

Daniel

View solution in original post

0 Kudos
Reply
3 Replies
1,092 Views
soledad
NXP Employee
NXP Employee

Hello Isao,

Are you using MQX for KSDK?

Regards

Sol

0 Kudos
Reply
1,092 Views
isaotakashima
Contributor IV

We don't decide to use which sample project.

If MQX for KSDK support USB Host isochronous transfer mode with the KL26, we can use it.

Please let us know which sample project supported as soon as possible.

Best regards,

Takashima

0 Kudos
Reply
1,093 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Takashima:

Yes, the KL26 device supports isochronous transfer. But due to the limited flash size, the host_audio_speaker example is not enabled for KL26. You can refer to the host_audio_speaker example of some other platforms, ie.K22, to try isochronous transfer.

Regards

Daniel

0 Kudos
Reply