Does MQX use the hardware watchdog

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MQX use the hardware watchdog

Jump to solution
1,422 Views
barbercolman
Contributor III

Hi

I am using MQX 3.7 and CW10.1 I have a project based on the gpio demo for the MFC51JM eval board. I am new to Freescale and MQX, but learning. As far as I can tell MQX has its own software watchdog but does not set or use the hardware watchdog. Is this correct? If it is correct any quide lines on using the watchdog? Does the BDSM debugger stop the hardware watchdog?

 

Any help or suggestions?

Thanks

0 Kudos
Reply
1 Solution
936 Views
DavidS
NXP Employee
NXP Employee

Hi Barber,

The FSLMQX3.7 doesn't yet support the JM128 on-chip watchdog but it is supported in the MCF52259 code.  I have tested it long ago but not recently as fyi.

If you look at the init_bsp.c file in the FSLMQX3.7/mqx/source/bsp/m52259evb _bsp_timer_isr() .

Hope this helps.

Regards,

David

View solution in original post

0 Kudos
Reply
1 Reply
937 Views
DavidS
NXP Employee
NXP Employee

Hi Barber,

The FSLMQX3.7 doesn't yet support the JM128 on-chip watchdog but it is supported in the MCF52259 code.  I have tested it long ago but not recently as fyi.

If you look at the init_bsp.c file in the FSLMQX3.7/mqx/source/bsp/m52259evb _bsp_timer_isr() .

Hope this helps.

Regards,

David

0 Kudos
Reply