Hello all,
I'm running MQX 4.1 on a TWR-K60F120M. I want to translate www.google.com to an IP address. To do that I'm enabling DNS. I want to make the DNS request to my router (wich is located at 172.16.0.1 --> 0xA1160001).
I define DNS parameters under source/if/dnshost.c the following way:
char DNS_Local_network_name[] = ".";
uint32_t DNS_CACHE_NAME_LIMIT = 0;
char DNS_Local_server_name[] = "";
DNS_SLIST_STRUCT DNS_Local_server_list[] =
{{DNS_Local_server_name, 0, 0xAC160001, 0, 0, 0, 0,
0, DNS_A, DNS_IN }};
DNS_SLIST_STRUCT *DNS_First_Local_server = &DNS_Local_server_list[0];
Then I call DNS_init() in my code.
After that I call gethostbyname() as you can see next:
HOSTENT_STRUCT_PTR CPTServer;
printf("Initializing DNS service...");
if(DNS_init() != RTCS_OK) {
printf("KO\n");
_task_block();
}
printf("OK\n");
printf("Resolving google.com");
CPTServer = gethostbyname("www.google.com.");
if(CPTServer == NULL) {
printf("KO\n");
_task_block();
}
printf("OK\n");
The code is running with no problems. But, how can I extract the IP from CPTServer?
Thanks in advance.
Óscar.
已解决! 转到解答。
Carlos's information very good.
I have implemented the below for my DNS example:
host = gethostbyname(string); if (host != NULL) { name = host->h_name; alias1 = host->h_aliases[0]; alias2 = host->h_aliases[1]; type = host->h_addrtype; length = host->h_length; ip = *(uint_32_ptr)host->h_addr_list[0]; printf (" %d.%d.%d.%d\n", IPBYTES(ip));
} else { printf("\nNo IP address found for given URL....try again please.\n"); }
Regards,
David
Hi Oscar,
I have recently used RTCS shell example:
C:\Freescale\Freescale_MQX_4_1\rtcs\examples\shell
The _README.txt file is very clear and it explains all the example services including DNS. With this example I was able to solve www.google.com IP address.
I hope it helps.
Regards,
Carlos
Carlos's information very good.
I have implemented the below for my DNS example:
host = gethostbyname(string); if (host != NULL) { name = host->h_name; alias1 = host->h_aliases[0]; alias2 = host->h_aliases[1]; type = host->h_addrtype; length = host->h_length; ip = *(uint_32_ptr)host->h_addr_list[0]; printf (" %d.%d.%d.%d\n", IPBYTES(ip));
} else { printf("\nNo IP address found for given URL....try again please.\n"); }
Regards,
David