DNS issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DNS issue

950 Views
aryavijayan
Contributor II

Hi,

 

We have observed that the DNS server is failing to resolve the IP address. This is mostly seen when we switch the router OFF/ON. But that time we can ping the DNS IP successfully. Note that other devices are working in the same network without issues. Please provide a solution.

 

Another question is should we start DNS client when we retrieve IP from DHCP server? We are using the below calls to get IP from DHCP server.

ipcfg_bind_dhcp_wait(),

dnsIPAddress = ipcfg_get_dns_ip(ENET_DEVICE,0)

 

Should I call ipcfg_add_dns_ip(ENET_DEVICE, dnsIPAddress ) after ipcfg_get_dns_ip()??

 

More details:

OS                     : MQX 4.0.2

Platform            : K60

Regards,
Arya

4 Replies

721 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Arya:

I would suggest you refer to MQX 4.2.0  and patched 4.2.0.2. In this version, we fixed one DNS bug, it seems related your issue.

pastedImage_1.png

Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button or helpful. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

721 Views
aryavijayan
Contributor II

Hi Daniel,

Thank you for the response.

Well, from where can I download patched version 4.2.0.2?  I couldn't find it in MQX™ Classic Software Solutions|NXP. Could you please share the link?

Thanks & Regards,
Arya

0 Kudos

721 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi arya vijayan

Please try this link

MQX™ Software Solutions - Releases and Patches|NXP 

pastedImage_3.png

Regards

Daniel


Have a nice day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

721 Views
aryavijayan
Contributor II

Hi Daniel,

Thank you so much!!

Regards,
Arya

0 Kudos