Copy from USB drive in MQX 4.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Copy from USB drive in MQX 4.1

1,077 次查看
acremonini
Contributor III

Hi,

I'm developing an MQX-based application on a K70 and I'm facing an issue:

I wrote a shell custom command to copy a directory from the USB drive to the NAND filesystem, including subdirectories and files, but sometimes, expecially when a large file is copied, the procedure ends and after that I can't see the content of the key anymore. However I see that the filesystem is still mounted (as "b:").

To check if the problem is inside my function or something else I tried the copy of a large file with the shell command "copy" and I see the same result. While debugging I noticed that the code fails during a read.

Does anybody have some suggestions about this or experienced something similar?

标签 (2)
0 项奖励
回复
1 回复

869 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi

Please check the following thread

Re: Copy a big file: Neither the shell command nor the custom code work

Regards

Daniel

0 项奖励
回复