Composite device with mqx usbd stack

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Composite device with mqx usbd stack

跳至解决方案
1,110 次查看
handychandra
Contributor III

Hi, i want to ask if it is possible to use mqx usbd stack to create usb device with two functions, say cdc and msd ? So computers will detect it as two device, cdc and msd.

标签 (1)
标记 (3)
1 解答
876 次查看
soledad
NXP Employee
NXP Employee

Hi Handy,

The theory says it is possible to use mqx usb stack to create usb device with cdc and msd, unfortunately we do not have an example to share with you based on MQX.

However, you can find MSD+CDC and HID+Audio+Video composite device examples that you could use as reference on bare-metal Freescale USB Stack v4.1, which can be found on www.freescale.com/medicalusb

Have a nice day!!!

Regards

Soledad

在原帖中查看解决方案

1 回复
877 次查看
soledad
NXP Employee
NXP Employee

Hi Handy,

The theory says it is possible to use mqx usb stack to create usb device with cdc and msd, unfortunately we do not have an example to share with you based on MQX.

However, you can find MSD+CDC and HID+Audio+Video composite device examples that you could use as reference on bare-metal Freescale USB Stack v4.1, which can be found on www.freescale.com/medicalusb

Have a nice day!!!

Regards

Soledad