I am working on using data pins to transmit data back and forth on a bus.
However I am having problems with changing the direction of the data pins from input to output and back.
I have tried using lwgpio_set_direction() but it doesn't seem to be working.
Any ideas?
Thanks in advance,
Derek
已解决! 转到解答。
Thank you for the reply Kamil,
I'm not so sure about initializing the pin again as the first parameter in lwgpio_set_direction() is: handle [in] - Pointer to the LWGPIO_STRUCT pre-initialized by lwgpio_init() function.
In respect to the pin being in gpio mode, I'll try taking it out of gpio mode, changing the direction, and setting the pin back in gpio mode.
I'll let you know how it goes.
Here's the relevant code. No this isn't how it looks, just putting the relevant information.
Define the data pins
| #define PIN_D0 | (GPIO_PORT_D | GPIO_PIN6) |
| #define PIN_D1 | (GPIO_PORT_D | GPIO_PIN5) |
| #define PIN_D2 | (GPIO_PORT_D | GPIO_PIN4) |
| #define PIN_D3 | (GPIO_PORT_D | GPIO_PIN3) |
| #define PIN_D4 | (GPIO_PORT_D | GPIO_PIN2) |
| #define PIN_D5 | (GPIO_PORT_C | GPIO_PIN17) |
| #define PIN_D6 | (GPIO_PORT_C | GPIO_PIN13) |
| #define PIN_D7 | (GPIO_PORT_C | GPIO_PIN9) |
#define MUX_GPIO (1)
| #define LOW | LWGPIO_VALUE_LOW |
| #define HIGH | LWGPIO_VALUE_HIGH |
Setup the pin structure
LWGPIO_STRUCT* dataPins[8];
LWGPIO_STRUCT D0;
LWGPIO_STRUCT D1;
LWGPIO_STRUCT D2;
LWGPIO_STRUCT D3;
LWGPIO_STRUCT D4;
LWGPIO_STRUCT D5;
LWGPIO_STRUCT D6;
LWGPIO_STRUCT D7;
Initialize the data pins as output for writing to the bus, all low
if (!lwgpio_init(&D0, PIN_D0, LWGPIO_DIR_OUTPUT, LOW))
success = 0;
if (!lwgpio_init(&D1, PIN_D1, LWGPIO_DIR_OUTPUT, LOW))
success = 0;
if (!lwgpio_init(&D2, PIN_D2, LWGPIO_DIR_OUTPUT, LOW))
success = 0;
if (!lwgpio_init(&D3, PIN_D3, LWGPIO_DIR_OUTPUT, LOW))
success = 0;
if (!lwgpio_init(&D4, PIN_D4, LWGPIO_DIR_OUTPUT, LOW))
success = 0;
if (!lwgpio_init(&D5, PIN_D5, LWGPIO_DIR_OUTPUT, LOW))
success = 0;
if (!lwgpio_init(&D6, PIN_D6, LWGPIO_DIR_OUTPUT, LOW))
success = 0;
if (!lwgpio_init(&D7, PIN_D7, LWGPIO_DIR_OUTPUT, LOW))
success = 0;
set gpio functionality
lwgpio_set_functionality(&D0, MUX_GPIO);
lwgpio_set_functionality(&D1, MUX_GPIO);
lwgpio_set_functionality(&D2, MUX_GPIO);
lwgpio_set_functionality(&D3, MUX_GPIO);
lwgpio_set_functionality(&D4, MUX_GPIO);
lwgpio_set_functionality(&D5, MUX_GPIO);
lwgpio_set_functionality(&D6, MUX_GPIO);
lwgpio_set_functionality(&D7, MUX_GPIO);
put pins in an array for easy usage
| dataPins [0] = &D0; |
dataPins [1] = &D1;
dataPins [2] = &D2;
dataPins [3] = &D3;
dataPins [4] = &D4;
dataPins [5] = &D5;
dataPins [6] = &D6;
dataPins [7] = &D7;
Then, if I want to read from the bus I change the direction with the following code
if (dataMode != READ) // make sure data pins are in input mode
{
dataMode = READ;
for (int i = 0; i < 8; i++)
{
lwgpio_set_direction(dataPins[i],LWGPIO_DIR_INPUT);
}
}
Hopefully this makes the situation a little clearer?
Hello Derek,
the description of lwgpio_set_direction() says that "..., it is possible to set the direction of a pin that is currently not in the GPIO mode." I think Your problem has to do something with that. As a second suggestion, I would say that You have to reinitialize with lwgpio_init() if You want to change the pin directions.
Have a nice day,
Kamil
Thank you for the reply Kamil,
I'm not so sure about initializing the pin again as the first parameter in lwgpio_set_direction() is: handle [in] - Pointer to the LWGPIO_STRUCT pre-initialized by lwgpio_init() function.
In respect to the pin being in gpio mode, I'll try taking it out of gpio mode, changing the direction, and setting the pin back in gpio mode.
I'll let you know how it goes.