Can you use and load both MQX 3.8.x and MQX 4.0.x with CW 10.3?
It seems like CW 10.3 defaults to what ever is installed first. Should one MQX be uninstalled?
Note: I can see both MQX 3.8 project and MQX 4.0 project under the "file>>new" menu selection.
Solved! Go to Solution.
Hi Colin,
You will be able to see both MQX in CodeWarrior, the issues will come up when you want to complile project for MQX 3.8. This is becuase MQX 4.0 replaces one Environment Variable called: "MQX_PATH". both versions are uisng the same variable. Just make sure you change it when you go from 4.0 to 3.8 and vise versa.
I hope this helps.
Regards,
-Garabo
Thanks! It is useful to know what path to change.
Hi Colin,
You will be able to see both MQX in CodeWarrior, the issues will come up when you want to complile project for MQX 3.8. This is becuase MQX 4.0 replaces one Environment Variable called: "MQX_PATH". both versions are uisng the same variable. Just make sure you change it when you go from 4.0 to 3.8 and vise versa.
I hope this helps.
Regards,
-Garabo
Hello Colin Dawson,
both of them should theoretically work. Why only theoretically, because CW 10.3 was released after these two MQX releases.
Could you detail more what do you mean with following line? "It seems like CW 10.3 defaults to what ever is installed first. Should one MQX be uninstalled?"
Regards,
MartinK