Can MQX be used on MCF51JM128?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can MQX be used on MCF51JM128?

Jump to solution
2,126 Views
wo_mig
Contributor I

Hello, everyone!

I am enagaged in developping a USB HOST device with based on MCF51JM128, which has the function of acciessing USB flash disk.

And now this is my question, can MQX be used on MCF51JM128?

0 Kudos
Reply
1 Solution
1,375 Views
wo_mig
Contributor I
0 Kudos
Reply
2 Replies
1,375 Views
DavidS
NXP Employee
NXP Employee

Hi Wo_mig,

The MCF51JM128 is supported in the latest Freescale MQX release on the EVB51JM128 evaluation board.

Best web site for FSLMQX info and downloads at:

http://www.freescale.com/mqx

Regards,

David

0 Kudos
Reply
1,376 Views
wo_mig
Contributor I
Thank you David
0 Kudos
Reply