Can I use the FNET V0.7.0 bootloader to my commercial projects?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use the FNET V0.7.0 bootloader to my commercial projects?

Jump to solution
1,541 Views
OOLife
Contributor III

 

Hi,

 

I want to know about FNET License policy.

 

That's hard to understand to me.

 

Can I use the FNET V0.7.0 bootloader to my commercial products or projects?

 

Could you guys explain about this more easily?

 

And, which is the best way to use FNET V0.7.0 legally with modification of FNET V0.7.0 ?

 

Thank you in advance

 

0 Kudos
Reply
1 Solution
864 Views
butok
NXP Employee
NXP Employee

Hi,

 

 

>> Can I use the FNET V0.7.0 bootloader to my commercial products or projects?
Yes, you can.

The FNET code http://fnet.sourceforge.net/ is under the GNU Lesser General Public License
http://www.gnu.org/licenses/lgpl.html.
Briefly, it means that you can do with FNET what ever you want, you should NOT open your proprietary code.
The only obligation is, if you do changes in the FNET source codes (fixes, improvements rtc.), you should open them, make them available to community (or send directly to the FNET project).

 

Best regards,
Andrey Butok

View solution in original post

0 Kudos
Reply
1 Reply
865 Views
butok
NXP Employee
NXP Employee

Hi,

 

 

>> Can I use the FNET V0.7.0 bootloader to my commercial products or projects?
Yes, you can.

The FNET code http://fnet.sourceforge.net/ is under the GNU Lesser General Public License
http://www.gnu.org/licenses/lgpl.html.
Briefly, it means that you can do with FNET what ever you want, you should NOT open your proprietary code.
The only obligation is, if you do changes in the FNET source codes (fixes, improvements rtc.), you should open them, make them available to community (or send directly to the FNET project).

 

Best regards,
Andrey Butok

0 Kudos
Reply