I’m are using MQX 4.1and a K20FX512VLQ12 connected to a Spansion S34ML08G2 NAND flash memory chip. Calls to IO_IOCTL_FREE_SPACE returns half the
memory size, 512K instead of 1MB.
I have updated the NANDFLASH_INFO_STRUCT to reflect the Spansion memory characteristics (page size, block size, etc…), updated
“wTotalInternalDice” in NFCNandMedia::initChipParam to show 2 dies on the chip. I’m sure I’ve missed a value that needs to be updated, but I’m not sure what it is.
Has anyone had experience setting up the BSP / FFS using a NAND memory chip that has two dies?
I’m using CodeWarrior 10.6 with MQX 4.1
Thank you.
已解决! 转到解答。
Hi Randall,
Could you please share here your NANDFLASH_INFO_STRUCT?
According my expectation, it should be:
/* S34ML08G2 organization */
#define S34ML08G2_PHYSICAL_PAGE_SIZE 2048
#define S34ML08G2_SPARE_AREA_SIZE 128
#define S34ML08G2_BLOCK_SIZE 131072 /* 128kB */
#define S34ML08G2_NUM_BLOCKS 8192 /*4096 for each 4 Gb device*/
#define S34ML08G2_WIDTH 8
NANDFLASH_INFO_STRUCT _ S34ML08G2_organization_8bit[] = {
S34ML08G2_PHYSICAL_PAGE_SIZE,
S34ML08G2_SPARE_AREA_SIZE,
S34ML08G2_BLOCK_SIZE,
S34ML08G2_NUM_BLOCKS,
S34ML08G2_WIDTH
};
Note: Unfortunately there is one additional FFS bug also in MQX 4.2.0. This could cause dead lock situation after some time.
In attachment you can find fixed media_buffer_manager.cpp file. Fix will be part of next MQX release.
I hope it helps you.
Have a great day,
RadekS
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Randall,
There was issue with FFS to NAND that had workaround of only letting you have access to 1/2 of the NAND space.
This was fixed in the MQX4.1.1 Release.
The Release Notes for it contain following:
MQX-4108 FFS NAND driver halves physical memory issue is fixed. The actual algorithm prepares enough reserved
blocks for a backup algorithm. The mfs_nandflash example is updated.
Updating should resolve the issue.
Regards,
David
David,
Thank you for your reply. I’ve updated to MQX 4.1.1 and have the same result, I even tried using MQX 4.2 but it also shows half the available memory which is what leads me to think I have missed something.
The Spansion memory is two 512 mega-byte planes per devices (in my post I mistakenly said 512K), I’m not sure where to tell MFS / FFS that there are two planes on the device.
Beside updating the NANDFLASH_INFO_STRUCT, NANDFLASH_INIT_STRUCT and wtotalInternalDice in initChipParm is there any other items you can think of I need to change?
Thank you for your time.
Randall Jordan
Hi Randall,
Could you please share here your NANDFLASH_INFO_STRUCT?
According my expectation, it should be:
/* S34ML08G2 organization */
#define S34ML08G2_PHYSICAL_PAGE_SIZE 2048
#define S34ML08G2_SPARE_AREA_SIZE 128
#define S34ML08G2_BLOCK_SIZE 131072 /* 128kB */
#define S34ML08G2_NUM_BLOCKS 8192 /*4096 for each 4 Gb device*/
#define S34ML08G2_WIDTH 8
NANDFLASH_INFO_STRUCT _ S34ML08G2_organization_8bit[] = {
S34ML08G2_PHYSICAL_PAGE_SIZE,
S34ML08G2_SPARE_AREA_SIZE,
S34ML08G2_BLOCK_SIZE,
S34ML08G2_NUM_BLOCKS,
S34ML08G2_WIDTH
};
Note: Unfortunately there is one additional FFS bug also in MQX 4.2.0. This could cause dead lock situation after some time.
In attachment you can find fixed media_buffer_manager.cpp file. Fix will be part of next MQX release.
I hope it helps you.
Have a great day,
RadekS
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Radeks,
Thank you for your reply. I must have misunderstood the structure setup, I have the number of blocks set to 4096, I was thinking that setting wTotalInternalDies to 2 would take care of the total number of blocks. I’ll make the change and post the results.
I’ve attached the NANDFLASH_INFO_STRUCT (with the total blocks changed to 8192) in case there are any other mistakes I’ve made.
Again, thanks for your help.
-Randy
Hi Randall,
You are welcome.
You are right,
I spend several minutes until my calculations returns 8192 blocks. I must agree that description of memory structure in MT29F2G16 datasheet is slightly better.
I hope it helps you.
Have a great day,
RadekS