I have installed both of the Patches for CW 10.1 and MQX 3.7. I created a new MQX 3.7 project through CW and built the project. I am receiving the #error below... Not sure where to go from here, any help would be appreciated. I have attached a jpg showing that the patches have been installed. Is there a way to find out what __CWBE__ is set to in my envrionment. Thanks again for any help.
#if (__arm__)
#if (__CWBE__ < 0x05000200)
#error You need to install Code Warrior V10.1 latest compiler patch. The code is unstable if patch is not used.
#endif
#endif
Solved! Go to Solution.
I have not managed to get any combination of updates to correct this problem yet. I'm uninstalling and re-installing now. (Note that I started from the CWX-MCU-PROED-EX version.)
Here is a jpg image showing that the updates have been installed...
Have you really updated the package? What i can see is that you just added repository of updates to your CodeWarrior.
Have you restarted your CodeWarrior after patch was applied?
Hi
I have equil issue.
But when I tried to update CW using Help->Install New Software.
I got error message:
An error occurred while collecting items to be installed session context wasprofile=PlatformProfile, phase=org.eclipse.equinox.internal.provisional.p2.engine.phases.Collect, operand=, action=). No repository found containing: org.eclipse.update.feature,com.freescale.coretech.debugger.kasample,7.15.0.FSL_b8910 No repository found containing: binary,com.freescale.coretech.debugger.kasample_root,7.15.0.FSL_b8910 No repository found containing: osgi.bundle,com.freescale.debugger.kernel.aware.sample,7.15.0.FSL_b8910 No repository found containing: osgi.bundle,com.freescale.debugger.kernel.aware.sample.corba,7.15.0.FSL_b8910
Could you give advice why I can't install this paches, please?
Best regards.