CW10.1 Secure Warning when flashing MQX Kinetis

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW10.1 Secure Warning when flashing MQX Kinetis

1,407 次查看
PetrL
NXP Employee
NXP Employee

There is an address space on Kinetis, the Flash Configuration Field, from 0x400 to 0x40F, that if written improperly can permanently secure the chip making it inaccessible. This is obviously dangerous. There is now a check in CW10.1 for linker files accessing this address space, which is a good thing. However, this check can result in false alarms. For example, even if the access to this data space is correct and OK, the alarm goes off because the data space is touched.

 

The MQX  3.7.0 default linker file was prepared such that the FCF address space is written using the correct and safe data (leaving the chip unsecured).  But after the CW10.1 1.0.1 update current MQX 3.7.0 customers will be bothered by this message every time they want to flash the MQX application. If you see this dialog (image below) you are safe to click "No" and continue the flashing operation.

 

 

 The problem will be fixed for a future release of the MQX RTOS and the CodeWarrior tools.

 

PetrL

0 项奖励
回复
3 回复数

950 次查看
NacuriErick
Contributor I

can you reattach the image please  ?

0 项奖励
回复

950 次查看
c0170
Senior Contributor III

Hello users,

 

this is the picture which has been missing here :

http://forums.freescale.com/freescale/attachments/freescale/kinetis/1602/2/secure%20warning.jpg

 

Regards,

MartinK

0 项奖励
回复

950 次查看
Mohsin455
Contributor IV

No image attached ?

 

Can ou please reattach it?

 

Regards,

Mohsin

0 项奖励
回复