Hi all, I'm using CW 10.3 professional and MQX 4.0. I updated CW 10.3 with the "com.freescale.mcu10_3.mqx_v4.0.win.v1_0_0" update to allow creating new MQX 4.0 projects, and built the MQX 4.0 libs with MQX_KERNEL_LOGGING =1 and my Processor Expert SSL App. When I break in the debugger, all the options under MQX are disabled, except "Check for Errors". When I hit that , it claims there is no data available. I had TAD working in CW 10.2 / MQX 3.8 , and I believe it was working under CW 10.3 before I installed the MQX 4.0 update. Anyone else have this problem?
Thanks,
John Reynolds
Solved! Go to Solution.
Hello john reynolds,
just in case you haven't read this thread: MQX 4.0 not showing in File/New in CW10.3
If that thread does not help you, let us know.
Regards,
0xco170
Martin, I now have the following sites enabled in my CW 10.3 updater preferences:
FSL MCU Eclipse Update Site http://freescale.com/lgfiles/updates/Eclipse/MCU10_3/com.freescale.mcu.updatesite FSL MCU Eclipse Update Site SSL http://freescale.com/lgfiles/updates/Eclipse/MCU/com.freescale.mcu.updatesite
I clicked Help|Install New Software and select the MCU 10.3 Updates and MCU 10.3 Updates for MQX, and it updated and I restarted CW. I ran my Coldfire Processor Expert SSL app, hit a break point, and as again, only the "Check for errors" is Enabled.When I click it, it still says "MQX Data is not currently valid." Clicking MQX|About MQX ka plugin states that I have Coldfire V4.6.2.2 installed. The only other options enabled in the MQX Menu is "Open System Browser"
Thanks for the help,
John Reynolds
John,
Have your project the OS Awareness enabled?
Luis
Luis, that was it. Either it got turned off somewhere, or I forgot that I had to manually set it because I never had a TAD problem before.
Thanks,
John Reynolds