Hi all, I'm using CW 10.3 professional and MQX 4.0. I updated CW 10.3 with the "com.freescale.mcu10_3.mqx_v4.0.win.v1_0_0" update to allow creating new MQX 4.0 projects, and built the MQX 4.0 libs with MQX_KERNEL_LOGGING =1 and my Processor Expert SSL App. When I break in the debugger, all the options under MQX are disabled, except "Check for Errors". When I hit that , it claims there is no data available. I had TAD working in CW 10.2 / MQX 3.8 , and I believe it was working under CW 10.3 before I installed the MQX 4.0 update. Anyone else have this problem?
Thanks,
John Reynolds
已解决! 转到解答。
Martin, I now have the following sites enabled in my CW 10.3 updater preferences:
FSL MCU Eclipse Update Site http://freescale.com/lgfiles/updates/Eclipse/MCU10_3/com.freescale.mcu.updatesite FSL MCU Eclipse Update Site SSL http://freescale.com/lgfiles/updates/Eclipse/MCU/com.freescale.mcu.updatesite
I clicked Help|Install New Software and select the MCU 10.3 Updates and MCU 10.3 Updates for MQX, and it updated and I restarted CW. I ran my Coldfire Processor Expert SSL app, hit a break point, and as again, only the "Check for errors" is Enabled.When I click it, it still says "MQX Data is not currently valid." Clicking MQX|About MQX ka plugin states that I have Coldfire V4.6.2.2 installed. The only other options enabled in the MQX Menu is "Open System Browser"
Thanks for the help,
John Reynolds