C# app will not communicate with K60 CDC example.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

C# app will not communicate with K60 CDC example.

4,772 Views
wpekrul
Contributor I

I have cloned the usb device virtual com example to my K60 board. It communicates fine with teraterm but will not talk to my c# application. I get the same results on win7 and xp. Any suggestions?

Labels (1)
Tags (1)
9 Replies

3,332 Views
Toe
Contributor IV

No response to this?  I have the same problem and it's holding me up.  I can see send packets through a terminal program and see the device respond as I expect, but when making a basic C# app the send never gets through.  I expect it might be some driver issue, but I haven't found it yet...

 

I'm using a JM128 with the 4.0.0 Freescale USB stack and driver.

 

0 Kudos
Reply

3,332 Views
FarhanH
Contributor III

I was having the same problem and found the answer in one of the other posts (don't have the link). If you are using the Processor Expert module from the USB Stack, then in your C# program set the following two SerialPort options to "true":

RtsEnable

DtrEnable

This will allow you to communicate using the C# SerialPort class without making any modifications to the firmware.

3,332 Views
kevinlfw
Contributor III

For anyone that comes across this in the future, I'm running the USB CDC Virtual COM demo found in KSDK 1.3.0 with my MK22F device and I was required to only set DtrEnable = true in my C# application. 

            m_SerialPort = new SerialPort("COM1", 115200, Parity.None, 8, StopBits.One)

            {

                DtrEnable = true

            };

If you set a breakpoint in the firmware, when start_transactions = TRUE, then you know the data will be received.

3,332 Views
PO220
Contributor IV

Thank you very much

Visual studio is a bit strange for Virtual com port...

I plucked my hair !

0 Kudos
Reply

3,332 Views
kevinlfw
Contributor III

I believe its the settings in the KSDK USB driver.  I've never had to set that property with a COM port/SerialPort over the 5 years I've worked with C# and heavy usage of SerialPort.  

If anybody is willing to take on the challenge, I'd be interested to know why DTR is required to be set, and a solution on how to edit the KSDK so its not required to be set, like most modern day COM devices.

0 Kudos
Reply

3,332 Views
BlackNight
NXP Employee
NXP Employee

Hello,

this is just a wild guess, but here is what I heard (I have not used C# myself), but I know that others reported a similar problem to me. The problem seems to be that the C# libraries seem to have a bug dealing with USB CDC. If I remember correctly, there should be a patch/fix from Microsoft available. Sorry, I do not have a pointer/link to this.

 

Otherwise, what I know is that sending too much data too fast causes problems with many USB CDC implementations. Try to add delays to the send/receive methods. Start with a slow data traffic, and find out if this 'fixes' your problem.

 

Hope this helps,

BK

0 Kudos
Reply

3,332 Views
Toe
Contributor IV

I'm not sure about that.  In the past I used the CMX usb stack and created a CDC project.  With that I didn't have any problems creating a windows app.  There are some differences between the descriptors for CMX and Freescale, though, and that's where I'm looking at the moment.

 

I may end up just going back to the CMX usb driver in the end.  We'll see...

0 Kudos
Reply

3,332 Views
BlackNight
NXP Employee
NXP Employee

Yes, it was just a shoot into the dark water from my side. I had used the CMX stack for ColdFire, and ended up fixing several bugs in the stack myself too (but using USB keyboard class).

I have used the FSL Stack, but faced strange problems with some buffer sizes as well (blocking terminal applications on the PC), see http://mcuoneclipse.wordpress.com/2012/04/17/fsl_usb_stack-updated-sending-16-or-32-byte-blocks/

That solved a lot problems for me. Not sure if this related.

 

Hope this helps,

BK

0 Kudos
Reply

3,332 Views
Toe
Contributor IV

That link ended up helping quite a bit. The CDC code in that PE module mentioned there has been modified quite a bit from the Freescale download.  I dug into it some and not only is it easier to set up, it doesn't have the problem wpekrul and I seemed to be describing when talking to the USB with C#.  I'm able to send and receive packets from my PC app now.

 

If I find some free time I'll spend a bit of it digging into the diffences, but at first glance it seems my expecation of descriptor issues isn't right.  For now, this will solve the problem I was having and let me finish up my PC app.

 

Thanks a ton BK!

0 Kudos
Reply