Building Libs w/ MQX 3.8 and IAR 6.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Building Libs w/ MQX 3.8 and IAR 6.5

ソリューションへジャンプ
3,765件の閲覧回数
jlag
Contributor II

I am attempting to build the TWRK60N512 libraries and I am receiving compiler errors on some macros in the assembly files using MQX 3.8 and IAR 6.5. The libraries build fine with IAR 6.4.

In the BSP:

iodebug_asm.s

line 80:

ASM_PUBLIC_BEGIN(ASM_PREFIX(_io_debug_semi_write_char))

Error[40]: Bad instruction

line 81:

ASM_PUBLIC_FUNC(ASM_PREFIX(_io_debug_semi_write_char))

Error[42]: Duplicate label:'CFI'

Error[114]: Directive is not allowed

Error[40]: Bad instruction

These errors repeat for other macros in the file. In the PSP file cortex_boot.s I have similar errors in the macros.

Any ideas are appreciated.

1 解決策
2,909件の閲覧回数
OldNick
Contributor IV

IAR changed - you now need a space as the first char on the ASM_PUBLIC lines

Hack the .s files today, and maybe MQX4 will have the neccessary changes tomorrow...we are all holding our breath for a bunch of new functionality in 4.

元の投稿で解決策を見る

7 返答(返信)
2,909件の閲覧回数
microeval
Contributor I

Hi All,

I have the same issue with MQX-Lite(Porting the KL46Z with MQX-Lite on IAR IDE). Created the MQX-Lite KL46Z project with Codewarrior IDE and included the MQXLITE source folder into IAR based KL46Z project.

Then while building:

boot.S

Error[40]: Bad instruction C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 39

Error[42]: Duplicate label:'.equ' C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 44

Error[40]: Bad instruction C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 44

Error[42]: Duplicate label:'.equ' C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 45

Error[40]: Bad instruction C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 45

Error[42]: Duplicate label:'.equ' C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 46

Error[40]: Bad instruction C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 46

how to resolve this error?  any suggestions..

Thanks in advance.

Regards,

--Ram.

0 件の賞賛
返信
2,909件の閲覧回数
danieldelatorre
Contributor IV

Your suggestion cleared it right up! Thanks.

0 件の賞賛
返信
2,909件の閲覧回数
jlag
Contributor II

Thanks all. Works fine now.

Seems like an IAR parse issue to me :smileyhappy:

0 件の賞賛
返信
2,909件の閲覧回数
OldNick
Contributor IV

Reply from IAR when we asked (last week) was

"This is not a bug in 6.50, but side effects of a bug fix made in 6.50.

  We had a bug in 6.40 that made it possible to place directives in the first position but this bug has now been fixed. The reason why this bug had to be fixed was that it made it impossible to use macros to create labels. This means that we will keep the requirement that directives defined by macros must not be placed at the first character position on the text line."


Glad all working

2,910件の閲覧回数
OldNick
Contributor IV

IAR changed - you now need a space as the first char on the ASM_PUBLIC lines

Hack the .s files today, and maybe MQX4 will have the neccessary changes tomorrow...we are all holding our breath for a bunch of new functionality in 4.

2,909件の閲覧回数
thomasmurphy
Contributor II

Also can confirm with MQX 3.8.1 for twrk60f120m on IAR 7.10.3.6832

This fix worked and the BSP now builds.

0 件の賞賛
返信
2,909件の閲覧回数
JuroV
NXP Employee
NXP Employee

Confirming, in MQX 4.0 we had to add space at the beginning.