Buffer for FFS MQX 4.0 K70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Buffer for FFS MQX 4.0 K70

Jump to solution
802 Views
Microfelix
Contributor IV

Hello

How long would like to know the size of the MFS cache to NAND flash memory.

This is because I have to upload files to 1 Mbyte 10 each and I have problems.

Do I have a fsclose to each file?

Maurizio

Tags (4)
1 Solution
609 Views
Martin_
NXP Employee
NXP Employee

I recommend to check the TAD to see how the memory is consumed per each open file. It is possible that you will need to fclose each file after application has completed its work with the file.

View solution in original post

1 Reply
610 Views
Martin_
NXP Employee
NXP Employee

I recommend to check the TAD to see how the memory is consumed per each open file. It is possible that you will need to fclose each file after application has completed its work with the file.