Hello!
I want to update my mcu software with serial port. So i created a bootloader using processor expert for uploading S19 records to flash. For testing a bootloader i created a test program with processor expert. The bootloader with the test programm works fine, but now i have problem with starting my main MQX application. I prepared the MQX project, but my main application doesn't start:
1) set vector table of main application to be placed in RAM in user_config.h and builded BSP and PSP libraries:
#define MQX_ROM_VECTORS 0
2) created new linker file:
shifted the adresses:
bootloader | (RX): ORIGIN = 0x00000000, LENGTH = 0x00003000 |
boot_flags | (RW): ORIGIN = 0x00003000, LENGTH = 0x00001000 |
vectorrom (RX): ORIGIN = 0x00004000, LENGTH = 0x00000410
/*cfmprotrom (R): ORIGIN = 0x00004400, LENGTH = 0x00000020*/
rom (RX): ORIGIN = 0x00004420, LENGTH = 0x0004BBE0 /* Code + Const data */
my_rom (RW): ORIGIN = 0x00050000, LENGTH = 0x00030000 /* my data */ |
ram (RW): ORIGIN = 0x1FFF0000, LENGTH = 0x00020000 /* SRAM - RW data */
/* kernel space starts after RAM variables (Location of MQX Kernel data + MQX heap) */
end_of_kd (RW): ORIGIN = 0x2000FFF0, LENGTH = 0x00000000
/* Boot stack reused by MQX Kernel data */
bstack (RW): ORIGIN = 0x2000FA00, LENGTH = 0x00000200 /* Boot stack */
end_bstack (RW): ORIGIN = 0x2000FC00, LENGTH = 0x00000000 /* Boot stack end address requires 4B alignment */
commented:
/*.cfmprotect :
{
KEEP(*(.cfmconfig))
. = ALIGN (0x8);
} > cfmprotrom*/
So i don't understand what i missed. Can anybody help me?
已解决! 转到解答。
The problem is solved.
Problem was in the stack pointer before initialization of MQX. Simmilar problem: Problem of initialization of MQX after jumping to the start of MQX application ( _boot() )
The problem is solved.
Problem was in the stack pointer before initialization of MQX. Simmilar problem: Problem of initialization of MQX after jumping to the start of MQX application ( _boot() )
Hi,
By default, MQX allocates the vector table at the first address of the flash memory, 0x0000-0000. Because this region of flash memory is used by the your bootloader, it will be necessary to reallocate the vector table in a RAM section.
I want to believe that this appnote can be a guideline for your application: http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4367.pdf
This appnote describes how to add the FNET bootloader to Kinetis projects. There is a section that includes adding it to the MQX linker which is the section that I believe you will find useful.
Have a great day,
Regards
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
I understand that reallocating vector table to the RAM is nessesary for MQX app to use it with bootloader. To allocate vector table in RAM we need to set in user_config.h:
#define MQX_ROM_VECTORS 0
I've already done it and rebuild BSP and PSP libraries. And vector table is in the RAM. The MQX application starts and works normal with the vector table in RAM, when i try to debug it without bootloader (with linker file without shifting memory sections). But this MQX application is not working when I use it with bootloader (with modified linker file that i have already posted). When i try to debug it with bootloader i jump to the correct addres in memory where __boot(); of MQX app exists. Start to execute programm, but then somewhere the MQX programm stops.
I tried to jump to __boot(); while debugging only MQX app without bootloader, and it starts normaly, but in main() while starting MQX in function _mqx( (MQX_INITIALIZATION_STRUCT_PTR) &MQX_init_struct ); crashes function _mem_zero((pointer) kernel_data, (_mem_size) sizeof(KERNEL_DATA_STRUCT));. And i don't understand why
I think that with bootloader the MQX app crashes in the same place.
And as have already said the test app created with processor expert without MQX starts and runs normaly.