I have a question about the best way to pass data into a task. I understand there is a message system for tasks, but I think the message system may be a bit overkill for what I'm trying to do. I have a board with multiple temperature sensors and I select which temperature sensor to read data from through a parameter I pass to 'temperatureRead' (see highlighted in red below). For example, to read temperature data from device 0, I call 'temperatureRead( 0 )'. To read temperature data from device 1, I call 'temperatureRead( 1 )'.
My question is whether or not my use of a global variable to specify the device (device 0, 1, 2, 3, 4, etc.) is the best way to accomplish what I am trying to accomplish. I like to avoid using global variables, but I also want a solution that is relatively simple.
void Temperature_task( uint32_t initial_data)
{
void *event_ptr; // Events are used to block tasks when not needed
if (_event_open("event.global", &event_ptr) != MQX_OK)
{
//TODO error message
}
while(TRUE)
{
// Go onto standby until a temp event is triggered
if (_event_wait_all_ticks(event_ptr, TEMP_EVENT_MASK, 0) != MQX_OK)
{
printf("\nEvent Wait failed");
_task_block();
}
// Lock the MUTEX to prevent too much communication across the I2C bus
if (_mutex_lock(&i2c_mutex) != MQX_OK)
{
printf("Mutex lock failed.\n");
_task_block();
}
temperatureRead( globalVariable );
_mutex_unlock(&i2c_mutex); // Unlock the I2C MUTEX so that other tasks can use the I2C bus
// Clear the event
if (_event_clear(event_ptr, TEMP_EVENT_MASK) != MQX_OK)
{
//TODO error message
} // end if( _event ...
} // end while(TRUE)
} // end Temperature_task
Thanks,
Mitty