BSP for MK60DN512 VLL10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSP for MK60DN512 VLL10

587 Views
mehdikarimibiuk
Contributor V

I have a new Kinetis MK60DN512 VLL10, which I will need RTOS for it. I believe for my MQX RTOS to work properly I would need proper BSP for it?

Where Can I get proper BSP for my MQX RTOS for my chip mentioned above?

I remember that I was trying to come up with my own bsp but I could not and the project softened to use of BareBoard with PE. I could never make a good bsp for an MQX 4.0 project in my CW10.5.

Now, I want to come back to RTOS using proper BSP. Can someone help me with this?

Thanks

Mehdi

Tags (3)
0 Kudos
2 Replies

370 Views
danielchen
NXP TechSupport
NXP TechSupport

There is an application note describes the difference between silicon 1.x and 2.x, you can check the following link for details

http://cache.freescale.com/files/32bit/doc/app_note/AN4445.pdf?&Parent_nodeId=&Parent_pageType=

0 Kudos

370 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Mehdi:

You can get proper BSP in MQX software package. The latest MQX version is 4.1. You can download it from the the link

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MQX&fpsp=1&tab=Design_Tools_Tab

In MQX 4.1, you will find two K60 bsp's.  twrk60n512 and twrk60d100. The first one is for silicon Rev1.x, the second one for silicon Rev 2.x.


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos