BSP clock configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

BSP clock configuration

跳至解决方案
1,246 次查看
davidsherman
Senior Contributor I

I have made a new BSP for the K10DN512VLL10 on a custom board.  Although there is an 16 MHz crystal on board, we are only using it for the CAN timing and just want to use the FEI mode at 96 MHz on the clock generator.  I've configured the MCG as such in _bsp_intialize_hardware in bsp_cm.c, however, things go wrong later in _bsp_pre_init().  It seems it's trying to use _bsp_osc_autotrim, which grossly throws off the slow internal clock (about 24kHz instead of 32.768).  So, what is the preferred way of specifying that I want clock configuration 0 to be FEI instead of PEE?  I don't wish to use PEE, since it can only get to 80MHz using the 16MHz crystal.  I could just disable the code, I'm just trying to understand how MQX intended to configure the clock.

0 项奖励
回复
1 解答
1,119 次查看
DavidS
NXP Employee
NXP Employee

Hi David,

I have had other customers just comment out or remove the autotrim code.

Regards,

David

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,120 次查看
DavidS
NXP Employee
NXP Employee

Hi David,

I have had other customers just comment out or remove the autotrim code.

Regards,

David

0 项奖励
回复
1,119 次查看
davidsherman
Senior Contributor I

Thank you David, I commented out the autotrim code.  I have it working now.

0 项奖励
回复