BSP Cloning Wizard unavailable in MQX 4.1 for K64F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BSP Cloning Wizard unavailable in MQX 4.1 for K64F

1,774件の閲覧回数
williamely
Contributor IV

Is this an oversight or intentional? It was available in the 4.0.2 version so why was it removed?

The K64 seems like a simple upgrade from the K60F family but it seems to be an entirely different beast.

タグ(2)
5 返答(返信)

1,439件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi William,

A workaround is to copy the MQX_4_1_TWRK64F120M folder contents into the MQX4_1_0_GA folder.

Then use the BSPCloning wizard to export the twrk64f120m to another path, generate the project for all or individual IDE.  Then close wizard.

Open the BSPCloning wizard in the new folder path and clone away.

Regards,

David

1,439件の閲覧回数
williamely
Contributor IV

Thanks David. I will give this a try in the next day or two.

0 件の賞賛
返信

1,439件の閲覧回数
markscovel
Contributor II

I had the same question and played around with it and eventually discovered that installing MQX_4_1_TWRK64F120M into the same folder that MQX4.1 installs into (instead of the default it wants to install into) will add the twrk64 board to the clone-able projects. If you find that the cloning wizard does not show your MQX4.1 path, go to Settings->preferences and edit the paths there to correct/add the right path.

It is also the case that you can open the cloning wizard and to to settings->preferences and edit or add a path to your MQX installation. apparently this is why the MK64 installation is not clone-able after installing (because the path that the cloning wizard is expecting is apparently corrupt).

1,439件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi William

The cloning wizard is an additional tool, it is not managed in git repo.  I will contact with the developers about this issue.

Thank you for reporting this.


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,439件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. MQX Software Solutions ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 件の賞賛
返信