Atheros AR4100P WiFi Driver for MQX4.1.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Atheros AR4100P WiFi Driver for MQX4.1.1

Jump to solution
1,973 Views
huishao2
Contributor IV

Hi-

Upgrading MQX3.8 legacy  SPI driver to newer driver from MQX 4.1.1, apparently AR4100P driver stops working. The newer SPI driver is needed as it supports multiple users to fopen() the shared SPI bus. Question is, is there a newer version of AR4100P wifi driver working with MQX 4.1.1 SPI driver? The most recent WiFi driver I can find is the R2.1 update 11 for MQX3.8. Will the support to WiFi on TWR board  be continued?

Thanks!

Hui

0 Kudos
Reply
1 Solution
1,667 Views
RadekS
NXP Employee
NXP Employee

You are right. It was dynamic link.

Please use this one: https://freescale.flexnetoperations.com/control/frse/product?child_plneID=683961&cert_num=178363021&...

and select MQX RTOS v4.0.2 releases and patches link.

I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
6 Replies
1,667 Views
RadekS
NXP Employee
NXP Employee

MQX Wifi patches are delivery by third party companies.

There is Qualcomm/Atheros AR4100 wifi patch for at MQX 4.0.2:

Please go to https://freescale.flexnetoperations.com/control/frse/product?child_plneID=683961&cert_num=178363021&...

and select MQX RTOS v4.0.2 releases and patches link.

NOTE: link edited.

MQX 4.0.2 already use new DSPI driver.

Unfortunately patch for newer MQX versions is not available.

I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,667 Views
huishao2
Contributor IV

Hi RadekS

I can't find anything to download from the link in your reply. Do you have a more specific link?

Thanks and regards

Hui

0 Kudos
Reply
1,668 Views
RadekS
NXP Employee
NXP Employee

You are right. It was dynamic link.

Please use this one: https://freescale.flexnetoperations.com/control/frse/product?child_plneID=683961&cert_num=178363021&...

and select MQX RTOS v4.0.2 releases and patches link.

I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,667 Views
huishao2
Contributor IV

The link always redirects me to

https://www.freescale.com/ruhp/myFreescale.html

where I don't see MQX 4.0.2.

thanks!

Hui

0 Kudos
Reply
1,667 Views
RadekS
NXP Employee
NXP Employee

I would like to apologize. It is again dynamic link. Grrrrrr….

Please go to http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MQX

Click on big Download button ion middle of page, on next page select Previous tab and select MQX RTOS v4.0.2 releases and patches link.

I hope it helps you.

Have a great day,
RadekS

1,667 Views
huishao2
Contributor IV

Realized that the previous link works with Chrome, I got it already.

Hui

0 Kudos
Reply