Assertion failed in MQX 4.1 FFS nandflash demo project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Assertion failed in MQX 4.1 FFS nandflash demo project

1,035 Views
dcantero
Contributor II

I´m running FFS NandFlash example proyect from MQX 4.1 using twrK60120 and the Demo reports the following problem (this is the output of the serial terminal):

This is the Flash File System example, type help for list of available commands

If this is the first time you use the demo, you should run "nanderasechip" command first.

Shell (build: May 21 2014)

Copyright (c) 2013 Freescale Semiconductor;

shell>

shell> nanderasechip

Erasing entire chip ...

Please use fsopen command to re-open NAND flash device.

shell> fsopen

assertion failed: logicalIndex < m_entryCount, file D:\Users\dcantero\Documents\

Electronica\MITO\Software\Freescale_MQX_4_1\ffs\source\wearleveling\ddi\common\page_order_map.cpp, line 169

Any idea about how to solve this issue?

Thnaks

Labels (1)
0 Kudos
Reply
3 Replies

646 Views
danielchen
NXP TechSupport
NXP TechSupport

since your log info is "logicalIndex < m_entryCount" ,  I suggest you print the variables.

646 Views
dcantero
Contributor II

Hi Daniel, thanks for your reply!!!

I did some tests after your answer and now everything goes well. I think the problem was that I have not installed MQX software in the "correct" path. A message about a TAD file have suddenly appeared and I have choose the file corresponding to K60. After that the demo have run like you described in the previous message!!

Thanks!!!!!

David Cantero      

0 Kudos
Reply

646 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi David:

I run this demo in my side. it can work. this is the output of the terminal

shell> nanderasechip

Erasing entire chip ...

Please use fsopen command to re-open NAND flash device.

shell> fsopen

NOT A DOS DISK! You must format to continue.

shell> format a:

Formatting...

Done. Volume name is

Free disk space: 12136 kB

shell>

shell> fsopen

NAND flash device was opened.

shell>


Have a great day,
Daniel

0 Kudos
Reply