Are there Updates to MQX to provide more Flash Drive Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there Updates to MQX to provide more Flash Drive Support

1,181 Views
Ali2006
Contributor II

Are there any updates files that can be added/integrated into MQX 3.8 to iprove the flash drive support.  I am currenlty using the Bootloader application for a K70 processor and while it does work about 1/2 of the USB sticks that I've tried do not get mounted to the devive.  I've seen the thread where people can post the results of there drives.. but I've not seen anywhere where we can get updates for our software to start supporting the drives that people have been providing..

Tags (1)
0 Kudos
Reply
3 Replies

960 Views
c0170
Senior Contributor III

Hello Ali2006,

we have tested tremendous amount of usb flash drives few weeks ago and all those changes in code are going to be reflected in new upcoming MQX 4.0, which is planning to be released next month. This should solve most of the problems if not all :smileyblush:

I am not aware of any update for 3.8 but you can diff changes with 4.0.

Regards,

MartinK

0 Kudos
Reply

960 Views
Ali2006
Contributor II

Thanks for the info..

Is there a firm release date set?

Can you give us any details as to what files we need to be concerned with to just update our flash drive support?

0 Kudos
Reply

960 Views
c0170
Senior Contributor III

Hello,

there's written early december in roadmap : MQX Roadmap

There were more files updated. I believe easiest way will be to update to 4.0 :smileywink: Or compare and try to update older MQX.

Regards,

MartinK

0 Kudos
Reply