Anyone have any information about FTP transfer rates on K6x family?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Anyone have any information about FTP transfer rates on K6x family?

1,678 Views
mscovel
Contributor III

We have RTCS, FTP and MFS running on a 180 MHz K65 with KSDK 1.3 (MQX).

We are finding FTP transfer rates around 14 K bytes//sec which seems slower than it should be.

We have removed all code except the above (commented out our application) and find that the best speed we can achieve is ~30 K bytes/sec.

Has anyone ever seen FTP performance rates above that on ANY K6x CPU?

Knowing what other have achieved will help us know if we have a problem we can fix.

Any help is much appreciated!

5 Replies

1,312 Views
fcw
Contributor IV

I don't have any server numbers, but I have a 96 MHz K64F client sending to a PC-based server at well over 100 KByte/sec. That rate with the server on the same 100 Mbit/sec subnet as the K64F client. This on a "classic" MQX 4.2 BSP-based implementation rather than KSDK. Data are sourced from either an SD card or a 1-bit wide SPI flash ROM, both bound to MFS.

1,312 Views
mscovel
Contributor III

Thank you very much Fred. Are you using RTCS or lwip or other? What FTP (embedded and PC app)?

0 Kudos
Reply

1,312 Views
fcw
Contributor IV

Using RTCS.

Servers are Bulletproof FTP and Filezilla. 

The client is a fair amount of application code around the client functions documented in the RTCS reference manual.

1,312 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Mark:

Is your board running as a server or as a client?

Regards

Daniel

0 Kudos
Reply

1,312 Views
mscovel
Contributor III

Our board is a server

Thanks

Mark Scovel

0 Kudos
Reply