Another problem about MQX.a

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Another problem about MQX.a

跳至解决方案
2,152 次查看
fish_yu
Contributor III
There is a file named MQX.a in MQX RTOS. I don't know which files are complied to output the lib file. Who could tell me Which files are complied to output the lib file?
I want to use MQX RTOS source code to make a project without any lib files about MQX. In fact, I want to design a project which only includes source codes to study MQX RTOS work. I compiled failed after using the files which are included BSP project and PSP project with hello.c which is in Example project in MQX directory. The Engineer of your Company told me that The MQX RTOS are full source codes.Could you help me how to solve the second problem?
Thank you for your help.
0 项奖励
回复
1 解答
1,414 次查看
Nouchi
Senior Contributor II

Hello,

 

Everything you need are located in C:\Program Files\Freescale\Freescale MQX 3.1\doc\mqx, you should have a look to MQXRM.pdf for MQX functions description, and MQXUG.pdf for how to use it, and take a special attention to chapter 5 (Developing a New BSP).

Kernel sources are located in C:\Program Files\Freescale\Freescale MQX 3.1\mqx\source folder.

 

 

Emmanuel

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,415 次查看
Nouchi
Senior Contributor II

Hello,

 

Everything you need are located in C:\Program Files\Freescale\Freescale MQX 3.1\doc\mqx, you should have a look to MQXRM.pdf for MQX functions description, and MQXUG.pdf for how to use it, and take a special attention to chapter 5 (Developing a New BSP).

Kernel sources are located in C:\Program Files\Freescale\Freescale MQX 3.1\mqx\source folder.

 

 

Emmanuel

0 项奖励
回复